你好!
请问一下,TPS54320 最大输出3A电流,可以这样理解11和12pin脚连接在一起输出电流不超过3A,还是11和12pin脚可以各输出3A?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
PH并非恒定的电流, 输出是能稳定的3A, 但是实际上因为电感的原因,电流是呈现三角变化的。
PH脚的电流和电感一致,大小并无意义(正常峰值会超过3A,可以认为是电流限制规格,见datasheet第6页参数表),芯片内部开关限制了最大电流,使得芯片最大输出电流为3A.