This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92641: 无输出,开关波形异常。

Part Number: TPS92641


Hi,

设计了一个36V输入,24V 1~8A输出多LED串并的驱动电路,原理图参照官方设计

开关频率设置为:416K左右

电感选用的18A饱和电流

当前未外接负载,IADJ输入为0.15V,理论上此时采样电阻上电流为1.5A

问题:

1. 虽然是空载,HG,SW,LG上的开关波形非常杂乱,尖峰过大,局部都超过FET的Gate耐压了

LG波形

HG上波形

这种情况一般是什么导致的呢?

Byron