Other Parts Discussed in Thread: NE555, LM3409
请教一下,我用一个PWM信号去调节LED亮度, 通过TLV733P输出3.3V到LED灯,TLV733P的使能脚为PWM信号,PWM频率1k到20kHz, 占空比0-100%. 请问这样可行吗,有没有损坏TLV733P的风险?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
不建议这样做,首先LED是恒流设计,不建议直接LDO供电导致电流不可控制,这样PWM调光就没有意义。
其次这类芯片EN能正常PWM调节频率不会很高,至多建议1kHz甚至更低,因为其启动时间就是几百uS.(而超过1kHz,周期就是1000uS)
Hi
大部分的LED 驱动频率都很低,因为一般调光频率都在200Hz左右。
如果要高频率调光,一般选择是LM3409, 但是用来做这个低压低电流看起来并不很合适。
而且如果是LED并联还要注意匹配的问题,因为VF如果不一致很容易出问题的。