This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25570EVM-206: 想问一下Vstor和Vbat的区别是什么?

Part Number: BQ25570EVM-206

进行能量收集的测试,但是想知道Vstor和Vbat的区别是什么,储能在哪呢?

  • 您好,

    VSTOR:Connection for the output of the boost charger. Connect at least a 4.7 µF capacitor in parallel with a 0.1 µF capacitor as close as possible to between this pin and pin 1 (VSS).

    VBAT:Connect a rechargeable storage element with at least 100uF of equivalent capacitance between this pin and either VSS pin.