This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400: 输入电压降低后TPS65400快速升温至140摄氏度以上

Part Number: TPS65400

你好,我们这边使用TPS65400,输入电压为12V。 通道1和通道2合并输出,通过调整可编程电阻器的阻值,改变RFB1的阻值,从而输出1.2-9.5V电压。通道3和通道4合并输出5V.。

我们在测试过程中发现,当通道1和通道2合并输出9.5V时,通过调整稳压源的输出电压可调旋钮,让TPS65400的输入电压从12V慢慢减小,降低到11V左右。通过使用红外测温仪就可以看到TPS65400的温度会快速升高。如果不及时断电,在持续高温状态下,TPS65400就会烧毁。在高温状态下,

请问有什么办法可以放置TPS65400在输入电压比较低的情况下烧毁吗

谢谢

Ryan

  • Hi

       应该已经工作到最大duty了,这个时候可能已经均流效果很差了,是否有电流勾表测量电流验证下?

       如果你只是想确认输出9.5V时,最低的输入电压,建议你避免这种情况, 保证输入的90%仍大于输出,并留有一点裕度。layout上输入电容尽量靠近对应Vin脚。