This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: LM5022 for PoE application

Part Number: LM5022


VIN=20~57V

VOUT=57V

Power Output =32W

Duty (VIN 57V) = 10%

Duty(VIN 20V)  = 34%

Efficiency (VIN 57V) =77%

Efficiency (VIN 20V) =88%

How could I tune duty for increase the efficiency (VIN 57V) ?