Part Number: TPS650864
Hi:
我使用的是TPS6508641
关于该器件我有3个问题想请教:
1、手册 6.10.1 CTLx Sequencing 提到“This allows the user to define up to six distinctive groups, to which each VR can be assigned for highly flexible power sequencing.” 也即可以自定义最多6个VR分组,然后使用CTLx进行控制,可是在寄存器描述中,我始终没有找到配置分组的方法,是我理解的有问题,还是说6508641这个具体型号无法进行配置?
2、手册 6.10.2 PG Sequencing 提到 “Any rail can be sequenced by the Power Good of a prior rail.” 这里上一个rail的PG触发下一个rail的使能,是通过芯片外部走线实现,还是芯片内部配置。从后文 “This can be combined with the CTLx method to allow for further sequence control and create more distinctive groups of enables than the six from CTLx.” 可以看出,应该是内部配置实现的。可是在寄存器描述中,我依旧无法找到配置方法。
3、我对TPS6508641进行I2C配置,在所有CTLx均为低电平时,对地址0xA0(I2C_RAIL_EN1)写0xff,可是读出来仍然是默认的0x00。I2C的读时序没有问题,都其它寄存器都可以。写时序通过示波器观察也没有问题。是我不可以直接修改该寄存器吗?还是我少了什么步骤?
盼回复,谢谢!