This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25616: 移除Vbus使用电池给VSYS后BATFET关断问题

Part Number: BQ25616


好。我司产品使用BQ25616,手持设备,锂离子电池供电。使用的时候移除充电器,使用25616的电源路径管理,电池通过batfet给到VSYS,VSYS给系统供电。当电池瞬间电压低于2.66V时,BATFET关断,系统断电。其实这个时候电池电压有3.6V,只是只是偶尔在LED灯打开的瞬间,电池电压上有一个下降的尖峰会降到2.6V,所以保护了。针对这种情况,请问有什么好的对策吗?在BAT与VSYS之间串一个二极管可以用?