This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: BQ78350-R1循环测试容量异常

Part Number: BQ78350-R1


尊敬的TI技术人员:

       我现在使用BQ78350-R1电量计,匹配电池组为15串的铁锂电池组,标称容量设置为10.8Ah,这组电池组我分别在常温和高温采用0.2C和0.5C和1C进行过老化测试,

做老化测试时,电池组实际容量更新是没有问题的(11.3Ah左右),但是我接着用0.2C循环测试5周来读取电池组的容量时,充放电后分别搁置时间为10分钟,

但我发现电池组容量与实际相差太大,第一周更改为10.3Ah,第二周更新为9.3Ah,第三周更新为低于9.3Ah,我设置FCC Learn UP和FCC Learn Down分别为1Ah,

      请问是什么原因导致这种容量更新不精准的情况?

      以上盼复!非常感谢。