This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: 误差放大器出错

Part Number: UCC28950


在使用UCC28950控制芯片时,EA-加参考电压2.5V,EA+加1.5V,VDD12V供电,CS端独调试控制芯片,但是当在误差放大器两端加载前述电压时,误差放大器的输出端电压COMP为4.2V,并不是EA+减EA-,进一步发现EA+固定为2.5V时,不管外加EA-为多大电压,COMP端均为4.2V,无法观测到输出A与输出C移相,并且上述现象出现时,SS端的电压是4.6V,应该工作在稳定模式,反向端输入电压应该就是EA-和SS端中较低的一个,1.5V。

请问出现上述问题原因?误差放大器的输出COMP不应该是EA+减EA-吗?