Part Number: TPS40055
输入电压为24V的TPS40055电源,拉载10A电流时,SW波形上升沿几乎没有过冲,下降沿反向过冲超限,为-2.6V,电流加大到15A时,反向过冲高达-3.8V,请问对于TPS40055这种同步整流的电源SW的反向过冲该怎么去抑制,或者说在设计时怎么使反向过冲最小?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS40055
输入电压为24V的TPS40055电源,拉载10A电流时,SW波形上升沿几乎没有过冲,下降沿反向过冲超限,为-2.6V,电流加大到15A时,反向过冲高达-3.8V,请问对于TPS40055这种同步整流的电源SW的反向过冲该怎么去抑制,或者说在设计时怎么使反向过冲最小?


Hi
这个我觉得一般是通过layout来避免,功率回路中的GND为0V(注意功率回路尽量小,GND走线尽量宽大点),在低边MOS启动瞬间,即便MOS体二极管先导通也只有0.7V的反向电压。而这个时候的GND(MOS的GND)与输入的大面积的GND layout相连,尽量保证GND上尽量小的noise,SW上就不应该有较大的反向电压。