Part Number: BQ25720
当前的许多功能有些复杂,请问有完整的方案嘛?
12.6v的充电电压,1.6A的充电电流,以及反馈电流和电压的读取,还有OTG的功能配置;
如果有的话,可以发送下,没有的话,我详细看看手册,后面也会贴出来代码
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ25720
当前的许多功能有些复杂,请问有完整的方案嘛?
12.6v的充电电压,1.6A的充电电流,以及反馈电流和电压的读取,还有OTG的功能配置;
如果有的话,可以发送下,没有的话,我详细看看手册,后面也会贴出来代码
您好,请参考数据手册Table 9-9. Charger Command Summary,具体哪个寄存器不更新。
您好,请参考数据手册9.6.16 ADCOption Register (SMBus address = 35h) [reset = 2000h],将对应的位使能。
i do it but no use ;最开始就配置好了
uint8_t Bq25720RegData[16][3]=
{//reg ,lowData,highData
{0x12,0x1c,0x87},
{0x14,0x40,0x06},
{0x15,0xF0,0x04},
{0x3B,0xFC,0x00},
{0x3C,0x00,0x0A},
{0x3D,0x00,0x00},
{0x3E,0x00,0x7A},
{0x3F,0x00,0x20},
{0x22,0x00,0x00},
{0x30,0x00,0x33},
{0x31,0xB7,0x00},
{0x32,0x34,0x04},
{0x33,0x09,0x4A},
{0x34,0xA0,0x41},
{0x35,0x43,0xC0},
{0x37,0x48,0x00},
};
您好,请参考下面链接,确认ADC设置成功。
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/885035/bq25703a-i2c-readback-registers-not-functioning/3273022?tisearch=e2e-sitesearch&keymatch=BQ25720%2520ADCOption%2520Register#3273022