This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5085: 电压问题

Part Number: LM5085

初次使用lm5085,电路采用webench的dc-dc电路图。电路设计设想是40v左右降压到12v,为后面芯片供电使用。

但是在使用时并不理想。电源模块焊接好后,刚通电测得gnd与电容正极电压为7点几伏,并且持续上升,最终上

升到与输入电压(40v)持平后,无法测得电压,同时pmos的g级测得无电压。请问这个大概是什么问题引起的。谢谢。

  • Hi

         将驱动信号波形传上来看一下?

         电路用webench仿真一般都是没有问题的,layout可以参考datasheet说明,但从你描述的现象看输出电压从7V上升到40V左右,是很奇怪的,首先建议你确认反馈与输出的焊接是否有问题,以及FB脚阻抗是否正常(断开测阻抗应该无穷大。

        其次请问你的芯片哪里买的?一般FB并不容易损坏,如果焊接没有问题,建议确认下芯片质量。