This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: 技术咨询

Part Number: UCC28950


你好,

   我们在使用UCC28950时,有如下疑惑,请帮忙解答一下,谢谢!

1. 当负载较轻时,芯片会进入Burst模式,导致输出电压纹波明显增大。最好的解决方案是什么?

2. 在轻负载下,芯片会进入Burst模式,例如:空载跳增至最大负载的80%,输出电压降比较深,如何快速退出Burst模式?如果是快速退出Burst模式,动态对我们是有帮助的。

3.脉冲模式在经过偶数个脉冲后停止。是什么决定了要传递的脉冲数(例如2或4)?

提示:Tmin对GND的电阻为10K。

  • Hi

       1. burst模式的纹波是应该要大一些,将输出电容再增加大一点看看效果。

       2.  快速切换datasheet没有提到,可能是内部控制,将SS减小看看有没有效果?

       3.  和负载有关。