你好,
目前在使用UCC28950时,遇到了一些问题,请帮忙解答一下,谢谢!
1. 当负载较轻时,芯片会进入Burst模式,导致输出电压纹波明显增大。最好的解决方案是什么?
2. 在轻负载下,芯片会进入Burst模式,例如:空载跳增至最大负载的80%,输出电压降比较深,如何快速退出Burst模式?如果是快速退出突发模式,动态对我们是有帮助的。
3.脉冲模式在经过偶数个脉冲后停止。是什么决定了要传递的脉冲数(例如2或4)?
提示:Tmin对GND的电阻为10K。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
1. burst模式的纹波是应该要大一些,将输出电容再增加大一点看看效果。
2. 快速切换datasheet没有提到,可能是内部控制,将SS减小看看有没有效果?
3. 和负载有关。