This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: 烦请提供TPS54331芯片的测试方法和测试判定标准,谢谢!

Part Number: TPS54331

型号:TPS54331DR,需要对TPS54331电源芯片的电路进行全面测试,但对其测试标准不是很了解,
- 烦请提供TPS54331芯片的测试方法和测试判定标准,谢谢!

  • Hi

        这个TI没有出文档说明的,但是可以参考datasheet或者EVM板的规格,例如datasheet 第14页这个案例,输出3.3V, 电压输出的规格可以定义为3.3V+/- 3%(一般电压范围tolerance是5%, 但是可以内缩一些),纹波小于30mV(一般小于输出电压1%),  然后可以测试一下过载保护,这个芯片最大输出3A, 你可以加载到4A,芯片需要在保护。

        (一般的电压测试,主要就是输出电压,输出纹波,以及过载保护,当然也可以增加一些,例如输入纹波)

  • 非常感谢!

    Have a good day!: )