This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: 上电发热,芯片不正常工作,测试FB脚输出0.1V左右

Part Number: LM5176


你好,

   我用LM5176设计了一款电源,今天开始能正常工作,在直接驱动大电机后再重新测试发现12V输入,输出只有1.6V左右,设计输出是13.8V,测试FB引脚电压只有0.1V左右,PGOOD输出低电平,而且芯片发热,VCC输出4V,是芯片烧了吗?如果芯片没有烧是哪里出问题?

    有什么办法测试芯片是否烧毁了吗?