老师您好!我司在使用bq27541-g1生产pack过程中发现,有部分电池的pack configuration参数项会出现变化,对比了一下DS,看到变化的具体位是CALEN位,对比了规格书中的解释,“bq27541-G1 Calibration mode is enabled. Default is 0”我这边异常的pack该位为1,正常电池该位为0,我想请问下老师,DS说明该位只是校准模型使能的,那CALEN值为1时候代表的是什么?通常情况下该位为1是否对我的PACK有影响?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
老师您好!我司在使用bq27541-g1生产pack过程中发现,有部分电池的pack configuration参数项会出现变化,对比了一下DS,看到变化的具体位是CALEN位,对比了规格书中的解释,“bq27541-G1 Calibration mode is enabled. Default is 0”我这边异常的pack该位为1,正常电池该位为0,我想请问下老师,DS说明该位只是校准模型使能的,那CALEN值为1时候代表的是什么?通常情况下该位为1是否对我的PACK有影响?
你好,请问在生产过程中是否进行了校准步骤?在按照Host System Calibration Method(SLUA640)是否还出现这个现象?
CALEN 可以使表示在校准状态,这个你可以看下CCA位是否也置起来,CCA位置位时CALEN位也会置位,并且观察CALEN位是否会清零,如果是这样子的话就是正常的。谢谢!