This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40200: 请问TPS40200这个芯片PWM控制芯片用吗?

Part Number: TPS40200
Other Parts Discussed in Thread: UC3844, , TPS40210, TPS40210-HT, LM5156H, UCC27712-Q1

请问TPS40200这个芯片可以当作UC3844的PWM控制功能用吗?想用TPS40200做一款高压600V输入,48V输出的电源。是高温电源,普通芯片耐温没那么高。

  • HI

        TPS40210是降压芯片,不能用作600V输入的电源转换,因为电压过高,超出很多pin脚的耐压。 如果你要选择类似UCC3844这样的反激芯片,是可以选择TPS40210-HT, 可以做成反激(最高210℃)。

        或者LM5156H系列,最高温度150℃

  •       感谢您的回复,我的电源功率额定120W,反激拓扑的功率基本到极限了,而且效率低,产品本身是高温环境下使用,后续的散热设计不好处理。

          UC3844是使用高压串联大电阻连接到VCC引脚,只要电流超过工作电流就行,请问下TPS40200能否这样使用呢?我想选择一款降压的高温PWM控制器,结果发现没有,就像用电源管理芯片去实现这个功能,不知道是否可行,麻烦帮忙分析下,非常感谢!

  • Hi

        单纯的非隔离方案应该是很难找到合适的芯片的,类似TPS40210,  外面只需要驱动一个高压MOS, 高电压并不会给到芯片上,即便是VDD也只是需要从高压上做个电压下来给芯片供电即可。 但是一般的buck芯片是很难左右。

        有些高低边半桥驱动芯片是可以做成同步buck的,例如UCC27712-Q1, 但是这个芯片最高结温是140℃, 同时还得找一个耐高温的控制芯片。