This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: 負載加載暫態時會有PWM 頻率變化造成過電流保護

Part Number: LM5122


各位好:

有一個問題請問

我設計一個300W Boost

輸入20~30V, 輸出50V

切換頻率100kHz(RT 91kOhm)

L: 47uH

Rsns=1.5mOhm

當Vin<23V時,  負載20%->80%會觸發current limit, 波形如下圖 CH1: 電感電流, CH2 Lo pin

我發現到在current limit triggered發生的時候, PWM 週期從9.4us變成6.5us(下一個PWM週期提早開),電感電流去磁不足, 造成電感電流衝上去觸發current limit

LM5122的頻率是由RT pin所設定, 為什麼會有頻率變化的問題?而且輸入電壓>23V並不會發生也不會觸發current limit

tek00000.tiftek00001.tif

感謝回覆