Part Number: BQ24168
我们根据BQ24168的规格书设计出来的电池过温充电保护电路跟电阻,做了实验发现电池表面在达到设定值(45°C)之后,还是能继续充电。我们设定电池充电温度为0°C-45°C,根据芯片上的公式以及NTC阻值对应表重新计算得R29约为9.8K,R30约为31K,实际板上应用的R29为10K,R30为33K。做了实验发现电池表面在超过45°C之后还是能充电,麻烦看一下我们的计算结果是否正确,如果不正确,请帮忙指出改善,谢谢。
根据芯片规格书设计的电路图如下(上面的阻值为之前设计的)。我们使用的电池里面带的NTC热敏电阻阻值为10K。