Part Number: TL2844B
Other Parts Discussed in Thread: TL431
1、Qsc什么作用,是否可以去掉2、Q1、DZ、RZ是否可以用电阻替代3、生成的参考设计中的阻容,我们会从现有物料库中选 值 相近的,改后是否有软件可以仿真一下TL431跟光耦组成的环路是否稳定。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
1. 谐波补偿电路,如果最大duty小于50%, 是可以不要这个电路的。反之必须要。
2. 这里是regalution, 通过稳压管做的一个固定电压。 但是很多设计光耦取电就是直接来自输出,通过电阻,所以是可以的。
3.尽量采用最接近的取值即可,一般小范围的差异应该是没有问题的。