This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952EVM: 芯片配置问题

Part Number: BQ76952EVM


芯片在BAT正负两端施加48V后直接进入正常模式,可以正常检测电池电压,添加负载后可以监测电流,主要问题如下

1、对寄存器进行配置写入时,芯片报错SCD,会直接关断MOS管,但此时SCD并未配置启动,无论写入任何寄存器都存在此问题;

2、对保护寄存器进行配置后,无法触发保护,例如CUV、COV等;

3、BREG电压仅有0.3V左右,REGIN电压为0,配置LDO后也没有输出;

4、TS2上电后电压为0.3V左右,直接退出shutdown进入正常工作模式,并没有按wake按键。