采用TPS82150作为顺序开启电源,根据手册LOGIC INTERFACE(EN), High-level input voltage(VIH)=0.9V(min)。代表EN有效的最小电压是0.9V?前一级的输出为1.0V(PG),是否可以作为下一级的EN,余量是否有点小,导致可能因为器件差异性,无法启动下一级电源?
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用TPS82150作为顺序开启电源,根据手册LOGIC INTERFACE(EN), High-level input voltage(VIH)=0.9V(min)。代表EN有效的最小电压是0.9V?前一级的输出为1.0V(PG),是否可以作为下一级的EN,余量是否有点小,导致可能因为器件差异性,无法启动下一级电源?
非常感谢!
Hi
是的,最低输入逻辑高电压为0.9V, 前一级PG电压1V是满足条件的,其中0.1V的gap是有些偏小但是并没有问题。但实际PG信号本身是上拉,你可以选择上拉更高一些的电压。