要求输出两路电压。压差控制在0.2V以内!一路输出3.3V左右,另一路输出2.8V左右!输入电压时3.6V和5V两种情况!5V的时候压差可以大点没关系。关键是电池供电的时候,压差一定要控制在0.2V以内!有没有这样的电源管理芯片!谢谢。公司急着开发项目!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输出电流需要多少??可以使用1.5A 的LDO TPS74001 (压差为0.1V)或TPS7A8001(压差为0.25V)