This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54227: 芯片烧坏咨询

Part Number: TPS54227

你好,

    我们在批量使用TPS54227过程中出现了多次烧坏芯片的问题:TPS54227芯片损坏,鼓包,14V、5V、GND之间短路。以下是相关的设计电路:

前两天发现有台机器编码器那里的+5V与本体外壳短路了,但因为外壳是浮地的,并没有影响正常功能,板子上的GND和外壳之前的压差是5V,这样的情况下机器也能正常工作。后面在这台机器上安装了另一个配件的时候,发现5V电源被拉低了,也就是电源短路了,可能是长时间短路导致芯片损坏。

   请帮忙分析一下损坏原因,以便规避这样的问题再次出现,谢谢!

  • Hi
        建议你首先从机构上避免,5V与外壳必须要隔离,这个应该也是有安规上的需要的,设备地不能和电源地短接,更加不能和电源(5V)短路,如果短路这样烧芯片很可能的。

        其次14V启动注意下,必须是软起动,不能有类似硬开关或者热插拔式的启动。