This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090: UCD9090烧录问题; 使用新版本TI-FUSION烧录工具可以正常显示烧录,但是烧录器断开产品重新上电后,程序无法从FLASH加载到RAM中运行。

Part Number: UCD9090


UDC9090烧录完成后,程序不运行;通过烧录器再次连接读写寄存器又是正常的,连接仿真器后程序又能正常运行。 

结论是:程序烧录正常,但是无法从FLASH中加载到RAM中运行。

1.使用TI-FUSION DIGITAL POWER DESIGNER 新版本7.4.1进行调试、修改寄存器,调试完成后进行烧录RAM TO FLASH;这时可以移除开发工具,UCD9090时序能正常输出。但是不能断电。

2. UCD9090 板子断开电源,再次重新上电,单独测试UCD9090板子无时序输出;重新连接DEMO,读出内部寄存器,各寄存器是正常的(芯片FLASH已经加载到RAM)

3.断开电源,将UCD9090板子移动到TI-FUSION DIGITAL POWER DESIGNER 老版本0.166,无法识别板子(NO DRIVES

无需重复烧录:将已经使用新版本7.4.1烧录的板子,重新启动,连接开发工具,再弹出的DEVICES ROM MODE 窗口中选择YES,板子内部程序开始工作,且正常输出时序,可以移除DEMO 板工具;但是断开电源再次重启,还是无法工作