请问各位技术专家,现在我要设计一个给8节锂电池组充电的恒流恒压充电电路,其输入范围是4v-50v,输出30v,2A。请问用什么芯片合适。TPS2010DGQ可以实现吗?或者是有没有适用于8节锂电池组的电池管理芯片可以使用啊。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS2010是power switcher,不能用来充电的。是指BQ2010吧,但BQ2010是电量管理的芯片,不是用来充电的。
可以使用BQ2954
http://focus.ti.com.cn/cn/download/aap/selectiontools/battery-chargers/tool.htm
guolin liang 说:你好,我在TI上看到一款电池充电器产品,他就是用TPS2010做的。只是它的输入范围没有这么低,但是我看TPS2010的手册发现它的输入是在4.5v到52v的。所以我想确定一下能否用它。你说的BQ2954可以用吗,我看看去。
http://www.ti.com.cn/product/cn/tps2010
请问你是在哪看到的输入是在4.5v到52v的??
TPS40210是升压器件,有可能实现恒压恒流,但需要另外加电路。
但在电池电压较低时,没有办法实现小电流的预充电,会缩短电池的寿命,建议使用专用的电池充电器。
BQ2954一般是用BUCK降压拓扑,没有办法实现宽电压范围输入的。可参考:
http://www.ti.com.cn/analog/cn/docs/litabsmultiplefilelist.tsp?literatureNumber=slua447&docCategoryId=1&familyId=411
http://www.ti.com.cn/analog/cn/docs/litabsmultiplefilelist.tsp?literatureNumber=slua070&docCategoryId=1&familyId=411