Other Parts Discussed in Thread: LM2587, LM5022, TPS40210
输入:18V-36V 标准24V
占空比:10%-60%
开关频率:210kHz
输出1:5V/4.5A
输出2:5V/0.5A
输出3:24V/0.1A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
输出1和输出2都是5V输出, 必须要做2路输出吗?
可以选择回扫式稳压器LM2587系列。
或者直接选择反激芯片LM5022, TPS40210之类。
Hi
上面推荐的芯片都是可以的,只是多个绕组出来。