第一组+-75V 15A,1kw
第二组+-20V
第三组+-15V
交流输入100-265V,隔离,是给音响供电,第三组的+-15V是开机用的,第二组是运放类供电,第一组是给功放供电。电路要精简一点,成本低一点。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
6组输出吗?一个变压器做起来估计很困难,第一组可以选择UCC28950 全桥移相(按照你的条件,第一组就超过2kW), 同时可以兼顾第二组输出。
第三组功率小可以选择UCC28610, 功率大可以选择UCC28600
Hi
关于电源电路的设计,如果你无法在芯片对应网站上找到参数一致的设计,你需要参照datasheet以及设计指导来设计,例如 www.ti.com.cn/.../slua560c.pdf