This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: 静态电流过大

Part Number: LM5175


Dear TI:

           LM5175在输入为24V时候静态电流有30mA,请推荐一款静态电流最小的芯片,输入18-36V,输出28V/6A。谢谢~~

  • Hi

       测试静态电流需要Vfb=0.9V,且此时Io=0mA.

       如果是测试空载功耗,且正常反馈(FB),  此时空载输入电流可能是mA级别,一般10~20mA是可能的,如果要减小,你需要确认选择尽量小Qg的MOS, 同时频率不要太高。

       LM5175是升降压芯片,大电流的升降压芯片并不好找。一般带有Powersaving模式(PFM)的控制芯片才会有很小的静态电流。

  • 开关频率设定为200K,模式选择DCM,静态耗流平均10mA以下,可以接受。