Hi Ti 工程师
我司某型号模块在上电测试时发现存在超过600mA的浪涌电流,使用的启动芯片为TPS22964,CIN输入电容为规格书推荐的1uF。验证发现浪涌电流取决于Cin电容大小,只有减小电容容值才能减小浪涌电流。请协助跟原厂确认以下问题:
- CIN允许的最小电容是多少?由1uF改为0.1uF会不会导致无法启动等应用风险?
- 根据规格书建议,输出电容Cout需要小于CIN。如果CIN更改为0.1uF,是否意味Cout需要选择更小的0.01uF?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti 工程师
我司某型号模块在上电测试时发现存在超过600mA的浪涌电流,使用的启动芯片为TPS22964,CIN输入电容为规格书推荐的1uF。验证发现浪涌电流取决于Cin电容大小,只有减小电容容值才能减小浪涌电流。请协助跟原厂确认以下问题:

HI
输入的1uF是防止芯片启动时瞬态拉低,而输出0.1uF是推荐,同时减小inrush电流。这里的inrush实际上是输入有电压,芯片on/off启动时的inrush,而不是输入电源启动时的inrush. 注意无论是前者还是后者都是软起动(类似MOS的开关控制,而不是硬开关或者热插拔式的启动)
输入电容可以适当减小,但是减小到0.1uF一些多,这个可能导致输入电压瞬态跌落(不能稳压),你可以根据负载实际情况通过测量结果来适当减小输入电压(输入不能有瞬态跌落)。
layout靠近是必须的,除了可以降低noise,还有稳压的需求。