This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54418高低温问题

Other Parts Discussed in Thread: TPS54418

你好,

我们的产品中使用了TPS54418做5V->1.0V和5V->3.0V的电源转换,但是在做低温实验(-40℃~-45℃)时,出现问题。

我们的电源的需求为:
输出电压为1.0V,最大输出电流为0.4A,瞬态电流变化相应ΔVout = 5%,切换频率为1MHz
输出电压为3.0V,最大输出电流为0.3A,瞬态电流变化相应ΔVout = 5%,切换频率为1MHz

测试现象为:
在低温环境下,我们的产品无法正常工作,我们使用直流电源从外部直接给后级电路输入1.0V和3.0V电源后,产品能够正常工作,因此判断为电源管理部分在低温下出现了问题。

附件是我们的原理图、关键器件料和PCB截图,见相关资料.doc。
请帮我们确认一下哪里出现了问题,谢谢!

祝工作顺利!

相关资料.doc