This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56637: 电感电容选型

Part Number: TPS56637


您好:

  tps56637规格书中对于输出电压及电感电容选型有一个List,想问一下按表中配置的话输入电压范围只要是4.5V~28V之内输出电压即为对应电压,电流为6A吗?

比如:Vout=5V  L=3.3uH Cout=30uF,Vin不管是12V还是24V或者是20V,输出都是5V 6A吗?

谢谢