This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS799: 如何理解TPS799数据手册上负载调整率和电压调整率?

Part Number: TPS799

请教大家:

在第一张图中TPS799的线性调整率为0.02 %/V,这是在说输入电压每变化1V,输出电压变化0.02%Vout ,还是说,是输入电压每变化1V,输出电压变化0.2mV?

同样的,负载调整率为0.002 %/mA,是说输出电流变化1mA,输出电压变化0.002%Vout ,还是说,输出电流变化1mA输出电压变化0.02mV?