Other Parts Discussed in Thread: TPS23881,
我们有个项目要做强供模式给非标的PD供电,之前使用的是tps23881,将其切换为manual mode,开启检测之后,强行供电可以成功,
后期因为缺料,只能换成tps23880,但是换成23880之后,模式切换不了,想写12h模式寄存器,寄存器的值一直是0XFF,写不进去
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
具体见datasheet第52页,对于四线对有线端口,两个通道必须设置为相同的工作模式。否则,端口将不会执行发现,并且将忽略所有开启命令。
我是4个通道都一起设置的,参数为0x7,0x7,SRAMCODE用的是01版本的
uint8_t tps_SetDevice4PPowerAllocation(uint8_t device_i2c_address,TPS238x_4P_Power_Allocation_t allocatepower12,TPS238x_4P_Power_Allocation_t allocatepower34) { uint8_t value; uint8_t rtn; value = 0x88 | (allocatepower34 << 4) |(allocatepower12); rtn = tps_WriteI2CReg (device_i2c_address,TPS238X_4PWIRED_POWER_ALLOCATION_CONFIG_COMMAND, value); return(rtn); }