This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79616-Q1: 我想使用BBP和BBN测量某一个电池串联铜排的电压,用于大电流充放电过程中的单体电压校正,但是发现BBP/BBN采样电压在输入电压为0时不为0,跟共摸电压正相关

Part Number: BQ79616-Q1


使用BBP和BBN测量母线电压,如果我把BBP和BBN直接短接,并将其固定在某一串电池上,会测量到0-3mV的电压,测量结果跟电池串数,也就是电池电压成正相关,比如接在第一个电池正,第二个电池正。。。第16电池正,BBP和BBN测量到的电压越来越大  最大越3mV,用万用表测量BBP和BBN之间的电压一直为0,。如果使用外接电源的方式为BBP和BBN之间提供电源,那么2mV的输入电压,测量值也是准确的。。说明测量误差是由于共模电压引起的??芯片内BBP和BBN内置差分放大电路的共模抑制比不够吗??有没有好的解决办法呢?