Part Number: TPS40200
器件回路都连接正常,需要输入12v输出8V,使用的就是手册提供的原理图,测量结果:在输入电压为12v时,FB引脚电压1.2V,COMP端电压为8v.将电压降低到5V,它在5-6V范围之内又可以稳压。但6V以上输出引脚就为高电平了,输出就不稳压了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
也就是输出6V一下可以正常,6V以上不稳定?
如果6V以上不稳定,你需要确认环路补偿(FB/Comp), 因为datasheet上电路,设置的3.3~5V输出,输出到8V,环路补偿很可能就不稳定了。(这种固定补偿的电路只适合小范围的输出变化,变化大了要调整补偿电路)
HI
也就是说输入电压高过8V, FB也跟着升高,即输出也跟着升高?但是不稳定。
如果是这样的话,你要确认layout, 参考一下datasheet上的说明。