This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用UC3843做电源的技术讨论

我用3843做了一个无变压器非隔离电源,LED驱动用的输入85-265v. 
36-48v400mA恒流输出,调试时3843不起振,用示波器测4脚6脚脉冲时有时无.想请高手们帮我出出主意

  • 可以先测试下8脚,查看5V参考电压是否建立,以确保3843没有欠压保护等其他异常。

  • 4、6脚脉冲时有时无,这是典型的384X重复启动过程,也就是384X的7脚电压充电到启动电压后,IC启动,输出脉冲,然后7脚电容放电到IC关闭,周而复始就是你看到的现象。建议如下:

    1、测量7脚波形,看是否如上所述,是否为一充电放电过程。

    2、你是否给384X的7脚提供了辅助绕组供电?

    3、如果提供了辅助绕组供电,7脚对地电容是多大的,增大该电容到47-100UF试试。

    4、如果还不行,请提供电路原理图及参数看看。