This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5164: LM5164

Part Number: LM5164


I use LM5164 to design, input 48V, output 12V, I design according to the official DEMO board, when I use the electronic load meter and DC stabilized source to debug, the waveform of the sw pin is normal, when I connect to the motherboard, it The SW pin waveform appears abnormal, similar to DCM mode, and then the inductor is whistling. How to solve this problem?