您好!
我们在使用TPS61071时,为了调整电路性能,尝试在反馈电阻R7上并联前馈电容C7,但原来没有C7时空载电流仅2mA,增加C7后空载电流增加到64mA(输出电压略有增加,从4.7V上升到4.95V)请帮忙分析一下原因及如何改善,谢谢


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
并非所有芯片都是适合增加这个前馈电容,并且前馈电容容值并不一定是10~200pF, 这个是要计算的,你可以参照:https://www.ti.com.cn/cn/lit/an/zhca058/zhca058.pdf
就你目前测试情况看,这个芯片似乎并不适合增加前馈电容,因为输出电压都出现明显过大的变化(0.25V的变化已经超过5%,这个已经是很大的变化),这个说明已经很大的影响反馈,甚至出现环路不稳定了。