Other Parts Discussed in Thread: TPS92200, TPS54200, TLC5917-Q1
能否帮忙推荐一款线性恒流源芯片,驱动8颗红外LED灯的方案,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS92200, TPS54200, TLC5917-Q1
能否帮忙推荐一款线性恒流源芯片,驱动8颗红外LED灯的方案,谢谢。
Hi
输入电压,输出电压,LED灯电流多少?
LED的结构(8串,还是有并联?)
你好!
电源电压是12V,因此输入电压12V以内都可以,输出电压没有要求。
LED灯的规格:Vf = 1.5V,If = 100mA
LED灯的结构优先并联方式,如果没有,可选串联方式;
谢谢!
Hi
并联主要的麻烦是VF匹配,如果可以并联,采用降压芯片比较容易做。
否者12V输出需要选择升降压设计,相对麻烦点。
例如可以选择TPS92200, TPS54200/1之类
不好意思,有一个需求没有讲清楚,我们这个对EMI比较敏感,不能用开关量的,只能用线性的。TPS92200和TPS54200/1都是带开关量的;
并联也可以先串后并,可以一路2颗或4颗,并4路或2路都可以,甚至可以采用多颗芯片来实现,都没有问题;
基于此,是否还有合适的推荐呢,谢谢。
Hi
看看TLC5917-Q1
只是如果你用这个芯片,建议你输入电压最好低一些,例如3V以内。
8通道的LED driver, 可以在里面选选,芯片并不多。