使用TPS2116DRLR做2路输入电源选择(使用2路稳压源),设置为VIN1优先模式,当VIN1输入电压降低到设定阈值电压时,出现VIN1和VIN2同时被打开的现象,两路电源都有电流,同时设备伴有轻微啸叫声,继续降低电压,超过设定电压后异常现象消失,电压从低升高现象也一样,请问这是什么原因造成的呢?
原理图如下:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
首先断电下测量2个通道是否有击穿的情况?
如果没有,PR1工作正常(要么就是高,要么就是低),仍然2通道导通,说明芯片工作不正常,应该已经损坏。
测试了,两个通道VIN1和VIN2,VIN1和OUT,VIN2和OUT均没有击穿的现象,我这边试了3个板子,现象都是一样的,测试了设置开关切换的值(VIN1为3V和VIN1为2.2V)两种情况,两通道同时有电流的情况都出现在VIN1到达临街切换值的时候,过了就正常了;
设计应用是将VIN1做为热插拔的外接电源,VIN2为电池供电一直保持连接(测试时使用2路稳压源模拟应用场景),
VIN1插入时,MODE为高,芯片工作在priorty mode,
VIN1拔出时,MODE通过PR1的分压电阻被拉低,芯片工作在如下模式,由VIN2供电;
麻烦看下,这样理解和应用有没有问题
Hi
有点不对呀,这个芯片是双通道实际就是MOS设计,如果2个通道都是导通的, 不同输入电压,只有一个输出电压,你怎么判定2个都导通呢? 按照你的测试是同时有电压输入时,同时有电流消耗,所以判定2个通道都导通。 例如3V/2.2V导通,输出3V就是第一通道导通,2.2V就是第二通道导通,但是这个时候实际输出是多少?
我这边没有测试板,不过你可以参考datasheet 第7页图6-1之类的时序来确认芯片功能。