This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25183: 是否可以在LM25183的SW端和变压器之间外接一个MOS管,减低芯片内部MOS的耐压

Part Number: LM25183

 ,请问是否可以在LM25183的SW端和变压器之间外接一个MOS管,减低芯片内部MOS的耐压。因为目前我24V输入,15V/0.5A输出时,芯片内部MOS管的Vds尖峰电压达到了60V,因此想通过外接源级驱动MOS,以分担芯片内部MOS管的电压压力,不知可否,如何可以,如何修改LM25183的外围参数,或者说LM25183的稳压机制是怎样的?

  • HI

        见过这类通过MOS叠加来增加受压的控制电路,但是这个芯片TI没有提供这样的方案(应该是TI基本上没有类似这种指导设计文档或者是参考电路)。

        但是就你目前的问题看,不需要这样设计,24V输入并不高,造成60V的尖峰电压却是很高,需要改善和降低这个电压,建议你确认一下变压器漏感是否太大?