如题,我的主控部分是锂电池供电,但是外边有个设备是poe供电的,功耗在2W左右,我看到ti 的poe 供电设备都需要48V以上的工作电压。请问有没有针对锂电池(8.4V)的解决方案?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,我的主控部分是锂电池供电,但是外边有个设备是poe供电的,功耗在2W左右,我看到ti 的poe 供电设备都需要48V以上的工作电压。请问有没有针对锂电池(8.4V)的解决方案?
POE供电是有IEEE标准规定的,PSE与PD间需要有满足一定的协议,PSE才能给PD供电。PSE与PD间是48V的,PD可以通过隔离与非隔离方案降压到所需要的电压。 http://wenku.baidu.com/view/6103ee8783d049649b665811.html
抱歉,我描述的不是很清楚。我是想做一个供电pse设备,但是pse供电设备的供电通过8.4V的锂电池供电的,而TI所有的pse芯片都需要48V的供电电源。 我想知道的是,是否有针对我这种用法的解决方案?还是说只能通过一个升压芯片将8.4V升到48V,然后再使用用pse芯片给pd供电?
你是想做PSE的供电电源?一般都是由一次电源来供的,个人的理解是PSE的输入端应该满足-48V通信电源的标准,输入应该要满足42V~58V,8.4V是不可以的
\shanqing liu 说:抱歉,我描述的不是很清楚。我是想做一个供电pse设备,但是pse供电设备的供电通过8.4V的锂电池供电的,而TI所有的pse芯片都需要48V的供电电源。 我想知道的是,是否有针对我这种用法的解决方案?还是说只能通过一个升压芯片将8.4V升到48V,然后再使用用pse芯片给pd供电?
能否说明下具体的应用?如果是2W多点的应用,使用POE供电已经没有什么优势。