This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: 充满电State Of Charge显示99% 不能到100% 电池容量8000mAh 3.7V

Part Number: BQ27426

 电池容量8000mAh  3.7V    

Design Capacity       7800

Design Energy          28860

Terminate Voltage     3200

Taper Rate                300

ID   1202   

做循环学习     数据显示都很准确  就是不能置位FC