Other Parts Discussed in Thread: TPS92640
从手册上看,可以得知lm3409并不直接驱动LED,而是同时pgate管脚输出控制信号驱动pmos管,所以lm3409所能支持的led功率大小应该就是由相应的pmos决定的吧。所以我能够使能lm3409来驱动总电流8A的LED吧,但是这又和主页上支持最大电流5A相悖了,有点疑惑,需要帮忙点醒一下。谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
一般推荐这款芯片设计最大电流5A(一般非同步的降压芯片最大电流设计通常是在5A左右,再大一般推荐用同步降压来做)。
就这个芯片而言,如果你要设计8A, 如上注意选择Qg尽量小的MOS, 同时重点确认layout。
或者选择TPS92640/1.
好的,明白了,谢谢@Johnsin Tao 。
同时,我会考虑TPS92640/1.