充电方案 :BUCK Charge BQ25601 + SC Charge SC8545 实现22.5W 充电, 现在出现充电BUCK IC 失效,目前分析初步定位到 下电VUSB 5V后,在VUSB端口还可以测试 4.2V 电源。导致系统还是识别充电器在位,但实际再次插入没有充电电流。请问该如何分析?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
也就是说输入的5V被拉低到4.2V? 此时是否有确认芯片损坏?
单片电池充电,如果你输入是4.2V, 电池是4.2V, 这样降压输出SYS是高于4.2V, 则buck就不会工作。
所以输入Vbus电压不能太低,或者拉低都是不能正常工作的。