Part Number: TPS62135
Other Parts Discussed in Thread: TPS56C215
Hi Team,
输入12V,输出5.5V。电感1.5uH。
客户目前设计上,TPS62135和TPS56C215输出内阻做到80mΩ,想做到40mΩ甚至更小。因为内阻小,减少输出波动,增加带载能力。TPS62135可以连续输出12A,我的设计只需要连续输出6A,内阻大了会导致请在到重载时电源波动大。
请问有没有设计建议可以使内阻做到40mΩ以下?或者参考设计?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你所说的内部是芯片内部MOS的Rdson, 这个和输出纹波没有关系,也和动态响应没有关系,如果要纹波尽量小,可以采用3个10uF代替输出22uF看看效果。
电容并联可以降低输出电容ESR,减小纹波。
Hi
如果是这样的话,一般DC/DC是很难实现的,即便是LDO 纹波也可能是2mV左右。
一般这类DC/DC纹波做的好可能在10mV~30mV, 轻载甚至到50mV.
建议你在输出增加以及LC,将纹波尽量降到最低,但是2mV还是有难度。