Part Number: TPS62740
Other Parts Discussed in Thread: TPS62742
TPS62740现在价格较贵,是否可以用TPS62742替代?或者有其他性价比更高的替代料吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
可以用TPS62742替代, 但是TPS62742可能购买更加贵,因为它是400mA的,而TPS62740是300mA版本。
芯片购买价格与数量有关,如果你购买的量较大,应该是可以获得更低的价格。
这个芯片价格看起来并不贵,如果要替代方案,pin脚兼容的应该是没有,只能找相同功能的可以吗?
你可以在里面将价格设置一个范围,例如小于0.4美元, 然后再看你的需求设置,例如输出负载能力,封装等等尽量缩小选择的范围,然后再细选。